SPRAC71B February 2019 – October 2023
The GC++ ABI requires that a static object referenced by an inline function be defined in a COMDAT group. If such an object has an associated guard variable, then the guard variable must also be defined in a COMDAT group. The GC++ABI permits the static variable and its guard variable to be in different groups, but discourages this practice. The C28x ABI forbids it altogether; the static variable and its guard variable must be defined in a single COMDAT group with the static variable's name as the signature.