SPRACA7A October   2017  – September 2022 TMS320F28075 , TMS320F28075-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S

 

  1.   C2000™ Hardware Built-In Self-Test
  2.   Trademarks
  3. 1Introduction
    1. 1.1 HWBIST Overview
      1. 1.1.1 HWBIST Working In-System
    2. 1.2 HWBIST Failure Response
    3. 1.3 Advantages of Using HWBIST In-System
  4. 2Using HWBIST In-System
    1. 2.1 Fundamental HWBIST Operation
      1. 2.1.1 Initializing the HWBIST Controller
      2. 2.1.2 Executing HWBIST
        1. 2.1.2.1 Executing HWBIST Micro-Run
        2. 2.1.2.2 Executing HWBIST Full-Run
      3. 2.1.3 Error Management
    2. 2.2 Managing HWBIST on Dual-Core Device
      1. 2.2.1 Semaphore Management
      2. 2.2.2 Interprocessor Communications
    3. 2.3 System Considerations When Using HWBIST
      1. 2.3.1 Interrupt Latency
      2. 2.3.2 Power Considerations
      3. 2.3.3 HWBIST Memory Requirements
      4. 2.3.4 Injecting Errors
    4. 2.4 Debugging HWBIST In-System
  5. 3References
  6. 4Revision History

HWBIST Memory Requirements

Three ranges of memory are reserved for HWBIST operation, as follows:

  • 32 words starting at CPU address 0x0000. This is the entry point that the boot ROM jumps to after a HWBIST reset and is used by the hwbist memory section. It cannot be moved to another address.
  • hwbiststack section used for a full context save and restore. It must reside within a SP addressable region. The size of the save/restore is different across device families. At most, like on F2838x, which needs to accommodate the FPU64 registers, 82 words are required.
  • Many of the HWBIST functions are placed in .TI.ramfunc for best performance. Size may vary slightly depending on device family and compiler version and options. You can remove the CODE_SECTION #pragmas from the HWBIST library files and rebuild the library if you prefer to have them execute from Flash.