SPRACC0A November 2017 – November 2020 TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1
C2000 are trademarks of Texas Instruments Incorporated.
All trademarks are the property of their respective owners.
With today’s significant reliance on electronic control and management comes concern for the safety of the electronic operation. One key point of concern is the operation of the SRAM in the system. This is important and from some perspectives, the most important aspect of safety in the execution of electronics. This is because:
For these reasons, SRAM bit cell and array layouts are key components to any new integrated circuit process development and qualification. It is where integrated circuit fabrication experts go to find drift and variation in manufacturing. This is why SRAM Error Detection is important in safety related electronics. If you would like to skip to the end, see Section 8.
The discussion includes:
Information is stored into SRAM as words. The word length varies per the needs of the storage. 32-bit words are used for this discussion. The bits of the word are stored in an array of bits. However, the physical position of each individual bit is optimized to the specifics of the semiconductor process. The array is a matrix with rows and columns. In the example below, there are N rows of 8 words each. If N = 256 that comes to 256x8x32 = 65,536 bits or 2048 words of SRAM.
Note how the bits of an individual word are not physically adjacent to each other, but rather all the bits of 1 D-input/Q-output are adjacent. The bits of an individual word are physically separated by 7 bits from other words. This improves both the size of the physical array and the routing of the D/Q signals. You will see later how this improves the error detect-ability of multi-bit failure mechanisms.
The following shows values in three words as follows:
Word(0) = 1 … 0 1b Row0, Column0
Word(1) = 1 … 1 0b Row0, Column1
Word(7) = 1 … 0 0b Row3, Column7
D0 | D1 | D31 | ||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
Row | Col | |||||||||||||||
0 | 1 | 2 | … | 7 | 0 | 1 | 2 | … | 7 | 0 | 1 | 2 | … | 7 | Column | |
N-1 | ||||||||||||||||
… | ||||||||||||||||
5 | ||||||||||||||||
4 | ||||||||||||||||
3 | 0 | 0 | 1 | |||||||||||||
2 | ||||||||||||||||
1 | ||||||||||||||||
0 | 1 | 0 | 0 | 1 | 1 | 1 |
The physical organization of bit cells in an array may vary for many reasons, but this figure provides a good example to discuss. This example shows a column multiplexor factor of 8, meaning there are 8 bits on a row for each Q/D. On a memory read the row is selected and then the column address provides the decode information for which specific bit will go out the Q. On a memory write, the column decodes define specifically which bits well be written to on the selected row. The sub-array (256x8) for each D/Q is called a stick.
Larger memory arrays are often organized with even higher column mux factors.