SPRACF4C June 2018 – January 2023 AWR1243 , AWR1443 , AWR1642 , AWR1843 , AWR1843AOP , AWR2243 , AWR2944 , AWR6843 , AWR6843AOP , IWR1843 , IWR6443 , IWR6843 , IWR6843AOP
If calibration reports are enabled using the rlRfRunTimeCalibConfig API, the AWR_RUN_TIME_CALIB_SUMMARY_REPORT_AE_SB asynchronous event message is sent by the mmWave device upon completion of any run-time calibrations (both one-time and periodic).
This report indicates the status of each enabled runtime calibration, and whether any calibration data were updated in the hardware as a result of the calibration. The report also contains the timestamp at which calibration was carried out, and the measured temperature at the time of calibration (this is the average of the temperature sensor readings from the temperature sensors located near the TX and RX channels).