SPRACF4C June 2018 – January 2023 AWR1243 , AWR1443 , AWR1642 , AWR1843 , AWR1843AOP , AWR2243 , AWR2944 , AWR6843 , AWR6843AOP , IWR1843 , IWR6443 , IWR6843 , IWR6843AOP
Figure 1-1 illustrates the radar front-end architecture in a TI mmWave radar device. The performance parameters of the RX LNA, IF amplifiers, TX PA, X4 (frequency multiplier), LO distribution buffers, and the clock sources shown all vary with process and temperature.
The purpose of calibrations is illustrated in Figure 1-2 using RX gain and TX power as examples. The gain of the RX LNA and the TX PA vary from device to device due to manufacturing process variations and also across temperature. The purpose of calibration is to ensure the RX gain and output power are maintained as configured by the user despite variations in process and temperature. To achieve this, the internal processor adjusts the mmWave circuit configurations at initialization (to mitigate effects of process variation) and periodically at runtime (to mitigate effects of temperature drifts). Figure 1-2 illustrates how calibration can be used to maintain the RX Gain and TX Power close to the configured settings across temperature drifts. These charts are illustrative and may not reflect actual device performance. Even with these calibrations done across temperature there would be some gain variations between devices, which must be considered in the user application.
These are representative plots on TI's first generation radar devices. Some of the calibrations (for example, the gain and power calibrations) are implemented as adjustments of circuit configurations based on measurement of RF/analog parameters. Other calibrations are implemented as adjustments based on process/temperature look up tables.