SPRACF4C June 2018 – January 2023 AWR1243 , AWR1443 , AWR1642 , AWR1843 , AWR1843AOP , AWR2243 , AWR2944 , AWR6843 , AWR6843AOP , IWR1843 , IWR6443 , IWR6843 , IWR6843AOP
For the duration required to complete the each of the bootime calibrations, run time calibrations, and monitors, refer to the Calibrations and Monitoring Durations section of the Interface Control document. Apart from the time for each of the calibrations and monitors, the firmware also has some fixed overheads which must be accounted for while computing the total interframe time requirements in an FTTI. These can be found in the Calibrations and Monitoring Durations section of the Interface Control document.