SPRACH9E November 2021 – February 2024 AWR1443 , AWR1642 , AWR1843 , AWR2544 , AWR2944 , AWR6843 , AWR6843AOP , IWR1443 , IWR1642 , IWR1843 , IWR6443 , IWR6843 , IWR6843AOP
The ROM bootloader performs the read from the FLASH based on the highest capability mode (quad, dual, or single) as published by the SFLASH in response to the SFDP command. The commands used are as published by the SFDP response. Thus, if the quad read is supported, the expectation is that the Quad Enable (QE) bit is already set in the FLASH. The ROM bootloader uses the quad mode to perform the read.