SPRACH9G November 2021 – December 2024 AWR1443 , AWR1642 , AWR1843 , AWR2544 , AWR2944 , AWR2944P , AWR6843 , AWR6843AOP , AWRL1432 , AWRL6432 , IWR1443 , IWR1642 , IWR1843 , IWR6443 , IWR6843 , IWR6843AOP , IWRL1432 , IWRL6432
The ROM bootloader in XWR1642 pre-production devices is not compatible with SFLASH variants that support extended addressing mode. In particular, the Number of Address length field of the SFDP command response being non-zero is not supported. The total SFLASH addressable region in XWR1642 devices is 8 MBytes. Thus, Number of Address length = 0 (corresponding to 3 bytes address length) satisfies the addressable range. However, the compatibility issue is with variants that allow for 3 or 4 bytes address length.
This incompatibility is addressed in the production version of the XWR1642 silicon.