SPRACJ6A October 2018 – December 2022 AM6526 , AM6528 , AM6546 , AM6548
The AM65x processors includes wide variety of capabilities, not all of which will be used in every design. Consequently, the requirements for different designs using the same device can vary widely depending on the target application. Designers must understand the requirements before determining the details of the design. In addition, the design may require additional circuitry to operate correctly in the target environment. For the selected device and determine the following, see latest device-specific collaterals on TI.com like the data sheet, Errata, TRM and EVM User's guides: