SPRACN0F October 2021 – March 2023 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The Hardware Built-In Self-Test (HWBIST) provides a very high diagnostic coverage on the CPU, including the FPU, TMU, and VCU, at a transistor level during start-up and application time. This logic utilizes Design for Test (DfT) structures inserted into the device for rapid execution of high quality manufacturing tests, but with an internal test engine rather than external automated test equipment (ATE). This technique has proven to be effective in providing high coverage in less time.
HWBIST tests are triggered by the software. The user may select to run all tests or only a subset of the tests based on the execution time allocated for the diagnostic. This time sliced test feature enables the HWBIST to be used effectively as a runtime diagnostic with execution of test in parallel with the application. HWBIST execution failure such as detection of a logic failure or time out without the self-test completing triggers an NMI. The maximum level of diagnostic coverage provided by HWBIST depends on the device as shown in HWBIST Supported Diagnostic Coverage by Device.
F2838xD/S | F2837xD/S | F2807x | F28002x |
---|---|---|---|
> 99% DC | > 99% DC | > 99% DC | > 99% DC |
To configure and run HWBIST it is required to use the HWBIST APIs provided by the C2000 Software Diagnostic library. The functions provided enable running a single micro-run or running the full HWBIST test as well as configuring a self-test mode within HWBIST to allow a few different types of faults to be injected to check that it’s functioning correctly.