SPRACO1A August   2019  – June 2024 F29H850TU , F29H859TU-Q1 , TMS320C28341 , TMS320C28342 , TMS320C28343 , TMS320C28343-Q1 , TMS320C28344 , TMS320C28345 , TMS320C28346 , TMS320C28346-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F2801 , TMS320F2801-Q1 , TMS320F28015 , TMS320F28016 , TMS320F28016-Q1 , TMS320F2802 , TMS320F2802-Q1 , TMS320F28020 , TMS320F280200 , TMS320F28021 , TMS320F28022 , TMS320F28022-Q1 , TMS320F280220 , TMS320F28023 , TMS320F28023-Q1 , TMS320F280230 , TMS320F28026 , TMS320F28026-Q1 , TMS320F28026F , TMS320F28027 , TMS320F28027-Q1 , TMS320F280270 , TMS320F28027F , TMS320F28027F-Q1 , TMS320F28030 , TMS320F28030-Q1 , TMS320F28031 , TMS320F28031-Q1 , TMS320F28032 , TMS320F28032-Q1 , TMS320F28033 , TMS320F28033-Q1 , TMS320F28034 , TMS320F28034-Q1 , TMS320F28035 , TMS320F28035-EP , TMS320F28035-Q1 , TMS320F28044 , TMS320F28050 , TMS320F28051 , TMS320F28052 , TMS320F28052-Q1 , TMS320F28052F , TMS320F28052F-Q1 , TMS320F28052M , TMS320F28052M-Q1 , TMS320F28053 , TMS320F28054 , TMS320F28054-Q1 , TMS320F28054F , TMS320F28054F-Q1 , TMS320F28054M , TMS320F28054M-Q1 , TMS320F28055 , TMS320F2806 , TMS320F2806-Q1 , TMS320F28062 , TMS320F28062-Q1 , TMS320F28062F , TMS320F28062F-Q1 , TMS320F28063 , TMS320F28064 , TMS320F28065 , TMS320F28066 , TMS320F28066-Q1 , TMS320F28067 , TMS320F28067-Q1 , TMS320F28068F , TMS320F28068M , TMS320F28069 , TMS320F28069-Q1 , TMS320F28069F , TMS320F28069F-Q1 , TMS320F28069M , TMS320F28069M-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F2809 , TMS320F2810 , TMS320F2810-Q1 , TMS320F2811 , TMS320F2811-Q1 , TMS320F2812 , TMS320F2812-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1 , TMS320LF2401A , TMS320LF2402A , TMS320LF2403A , TMS320LF2406A , TMS320LF2407A

 

  1.   1
  2.   Development Tool Versions for C2000 Support
  3.   Trademarks
  4. 1Introduction
  5. 2Code Composer Studio
  6. 3Codegen Tools Versions
  7. 4SYS/BIOS and DSP/BIOS Versions
  8. 5References
  9. 6Revision History

SYS/BIOS and DSP/BIOS Versions

Table 4-1 lists the minimum versions of DSP/BIOS and SYS/BIOS that support different C28x devices. The recommended version is always the latest release that supports the device. In addition to consulting this table, always check for critical updates and bug fixes.

Table 4-1 Required/Recommended DSP/BIOS and SYS/BIOS Support by Device
DeviceDSP/BIOS 5SYS/BIOS 6
240xNot SupportedNot Supported
281x5.41.02.14 or later(4)Recommend: 6.32 or later(5)
280x/2801x/280445.41.02.14 or later(4)Recommend: 6.32 or later(5)
2833x5.41.02.14 or later(1)(4)Recommend: 6.32 or later(3)(5)
2834x5.41.02.14 or later(1)(4)Recommend: 6.32 or later(5)
2823x5.41.02.14 or later(4)Recommend: 6.32 or later(5)
2802x5.41.02.14 or later(2)(4)Recommend: 6.32 or later(5)
2803x5.41.02.14 or later(2)(4)Recommend: 6.32 or later(5)
2805x5_41_12_40 or later6_33_02_31 or later
2806x5.41.10.36 or later6.32 or later
28M35xNot Supported6.32.03.43 or later
2837xDNot Supported
  • If using the ROM image of SYS/BIOS then use SYS/BIOS 6.37.01.04 with XDCtools 3.25.05.94
  • IPC for F2837xD are supported in TI-RTOS version 2.10.01, available by the end of November 2014
2837xSNot Supported
  • If using the ROM image of SYS/BIOS then use SYS/BIOS 6.37.05
  • If not using the ROM image of SYS/BIOS, then use 6.41.00 or later
2807xNot Supported
  • If using the ROM image of SYS/BIOS then use SYS/BIOS 6.37.05
  • If not using the ROM image of SYS/BIOS, then use 6.41.00 or later
28004xNot Supported
  • If using the ROM image of SYS/BIOS then use SYS/BIOS 6.42.01.10
  • If not using the ROM image of SYS/BIOS, then use 6.45.00.20 or later
2838xD/2838xSNot Supportedv6.76.01.12 or later
There is a critical C28x fix for FPU code in 5.33.03. SDOCM00050676 dispatcher for 2833x saves 'RB' register with interrupts enabled -- can cause random app failure.
5.33.06 Fixed: SDOCM00059875 Kernel Object View results in message "DSP/BIOS not initialized" on 2802x and 2803x devices.
ezdsp28335 users are recommended to use f28335dspbios.gel file supplied with CCSv4 to connect and load any BIOS example programs that require external memory.
5.41.02.14: Earlier versions have a critical NMI race condition that is fixed in this patch. SDOCM00064320 28x - NMI can cause race condition in BIOS 5 kernel (small code window where user can not return from NMI safely)
Support was added in 6.20, but significant enhancements were made in SYS/BIOS 6.32 to better support 28x devices. See SYS/BIOS for the 28x for more information.