SPRACP7 October 2019 AM6526 , AM6528 , AM6546 , AM6548
In real systems, it is important to have secondary time masters or hold-over mechanisms when the primary time master is not available, or when the communication channel is broken. Since AM64xx time-sync architecture allows delta adjustment to a local clock source, it is natural to maintain the same adjustment values during the period when no new adjustment values are available.
In case of loss of primary time master, the AM65xx device can be designated as the backup time master, where it can seamlessly resume the role of distributing master time bases. When the primary time master resumes, the secondary time master can hand-off the mastership to the primary. Detailed handoff mechanisms should be designed to ensure that certain time bases do not roll back.