SPRACT8 September 2020 66AK2H06 , 66AK2H12 , 66AK2H14
An out file called NIMU_FtpExample_EVMK2H_armExampleProject.out should be built. The example runs as the FTP server with a default IP address 192.168.1.4 on the K2H EVM. The PC acts as the FTP client with an IP address 192.168.1.11 as an example. The major test steps include:
A sample test screenshot shown in Figure 3-5, showing the PC test commands and FTP throughput reported. This proves the functionality of the K2H FTP server example. Note that the server does not really host a file system on the K2H EVM, get/put commands are simply memory operations.