SPRACU1A October 2020 – June 2021 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6441 , AM6442
The region of the PCB used for DDR4 circuitry must be isolated from other signals. The DDR4 keepout region is defined for this purpose and is shown in Figure 2-4. The size of this region varies with the placement and DDR routing. Non-DDR4 signals should not be routed on the DDR signal layers within the DDR4 keepout region. Non-DDR4 signals may be routed in this region only if they are routed on other layers separated from the DDR signal layers by a ground layer. No breaks are allowed in the reference ground layers in this region. In addition, a solid VDDS_DDR power plane should exist across the entire keepout region.