SPRACU1A October 2020 – June 2021 AM2431 , AM2432 , AM2434 , AM6411 , AM6412 , AM6421 , AM6441 , AM6442
This section discusses implementations (also called topologies) using single-rank x16 and x8 SDRAM devices. This section does not discuss recommendations for implementations that support low-power operation, such as when the SDRAM is held in self-refresh and the processor is powered off. It also does not discuss the DDR-less implementations. These options are under study and may be supported in future versions of this document.