SPRACU7A December 2020 – March 2021 TDA4VM , TDA4VM-Q1
Application app_single_cam starts with DCC database from sensor driver header file. This can be overridden at runtime by reading DCC binary files from file system on the SD card. app_single_cam has a runtime menu as shown below
" =========================="
" Demo : Single Camera w/ 2A"
" =========================="
" p: Print performance statistics"
" s: Save Sensor RAW, VISS Output and H3A output images to File System"
""
" e: Export performance statistics"
" u: Update DCC from File System"
" x: Exit"
" Enter Choice: "
Option ‘u’ instructs the application to find the DCC binary files in the folder:
/opt/vision_apps/dcc/<sensor_name>/<wdr_mode>
Where
Before giving the command ‘u’, make sure that this folder exists and contains the DCC files in binary format. If this folder contains partial DCC database, then only that part will be overridden. Example:
/opt/vision_apps/dcc/IMX390-UB953_D3/wdr/