SPRACU8B August 2021 – January 2023 AM68 , AM68 , AM68A , AM68A , AM69 , AM69 , AM69A , AM69A , DRA821U , DRA821U , DRA829V , DRA829V , TDA4VM , TDA4VM
In addition to the latency parameters, there are several additional DDR timings that need to be input into the Jacinto 7 DDRSS Register Configuration Tool. All of these parameters should be set based on the values obtained from the specific DDR component data sheet.