SPRACV2 November 2020 AWR1843 , AWR2243
Slight imbalances in the PCB routing of the 80-GHz TX and RX lines as well as the 20-GHz (FMCW Sync LO) lines are possible in cascade sensors with large antenna arrays. The TX, RX, and 20-GHz LO circuits in different devices can also have manufacturing variability. These can result in inter-channel imbalances across devices in the cascade systems.
It is common for customers to perform factory calibrations to measure the cascade’s inter-channel imbalances and TX phase shift errors, and store them in a non-volatile memory (NVM) for use in error compensation in-field. For this to be effective, the devices’ analog configurations (i.e., RF register settings) during in-field operation need to match those during factory calibration.
RF INIT calibrations can converge to different analog configurations each time they are executed due to measurement noises and temperature differences across executions. Therefore, triggering RF INIT calibrations in-field on every power cycle (as in single-chip context) can render the devices’ analog configurations to be different from those during factory calibration and make the factory calibration based compensation ineffective. As a way to avoid such a situation, TI recommends that each AWR device’s RF INIT calibrations are triggered only during the customer factory calibration process. Those results may be stored in a non-volatile memory on the sensor and restored to the AWR devices upon each power up during in-field operation.