SPRACV2 November 2020 AWR1843 , AWR2243
At the time of power up in the field, the host processor in the sensor may restore each device to the same RF INIT calibration state as at the customer factory. This can be done using the following procedure. It has slight deviations from the normal RF INIT call and start up sequence.
The above restoration does not include TX phase shift calibrations and digital delay compensation settings.
Because all calibrations are disabled in the above procedure, the calibration report API messages (AWR AE RF INITCALIBSTATUS SB) also reports all calibration statuses as 0. The mandatory calibrations (e.g. to keep the PLLs in lock) are done without host control. Unlike the timing constraint on issuing RF INIT API to all devices in the cascade in a non-overlapping manner during factory calibration and saving (to avoid mutual interference), there is no special timing constraint in the restore phase (because calibration measurements are actually disabled here).