SPRACV2 November 2020 AWR1843 , AWR2243
The TX phase shift factory calibration results (found in Equation 1 or Equation 2) can be restored to the AWR device using AWR PHASE SHIFTER CAL DATA RESTORE SB.
For restoring customer factory corner reflector based phase shifter calibration values, send the following to the above API:
For restoring values based on RF INIT TX phase shifter calibration executed in customer factory in to the device, send the following to the above API:
The user should account for this API’s phase indexing format, which may differ across TXs (refer to Table 7-5 and Table 7-6.
For simplicity of explanation, it is assumed here that the temperature at power up matches the factory calibration temperature. This assumption is not necessary and if wrong, the required steps are explained in detail in Section 3.5.4.