SPRACV2 November 2020 AWR1843 , AWR2243
In the AWR2243 cascade system, the 20-GHz LO signal from ClockOut or SyncOut pin of Master is routed on the PCB and fed to the SyncIn pin of all the devices, to achieve RF synchronization. This PCB routing can lead to losses in the 20-GHz Sync Path, and the change in 20-GHz SyncIn power level can indirectly change the TX Phase Shifter properties.
In TI lab evaluation of few devices across DoE process corners and temperature, with SyncIn BGA power set at approximately -0.5 dBm to -4.5 dBm, the change observed in PS INL with all the above recommended procedures and LUTs has been observed to be <1 degree across all phase shifter settings.
Because the 20-GHz power levels are highly dependent on the customer’s PCB design, if further TX phase shifter accuracy improvement is desired, the customer may consider characterizing the TX phase shifter over temperature across several of their own sensors, re-evaluating and re-deriving the LUTs mentioned in this note corresponding to their own sensor.