SPRACV2 November 2020 AWR1843 , AWR2243
The AWR PHASE SHIFTER CAL DATA RESTORE SB message should be issued to the device only when the radar frames are not ongoing, i.e. after issuing the issue the FRAME STOP command (using AWR FRAMESTARTSTOP CONF SB) and before issuing the next FRAME START command. If the customer desires to issue the AWR PHASE SHIFTER CAL DATA RESTORE SB without stopping the frame, then the host is responsible to ensure that the API is issued not when active frames are ongoing. This is true for both AWR1843 and AWR2243.