The necessary hardware equipment to
perform ISP tuning for a raw camera includes:
- AM62A Starter
Kit EVM (SK EVM) or a custom board with the AM62A SOC. For the
complete EVM setup, see the AM62A SK EVM Quick Start Guide.
- The camera and all necessary
accessories to connect the camera to the AM62A SK EVM. For how to connect the
camera to the EVM, see the AM62A Academy. From the Academy main page, go to Evaluating
Linux → Tour of TI Linux → Camera.
- A light box:
- With calibrated light
sources, typically ranging from 2700K to 6500K at least
- More light sources are
needed if wider range of color temperatures is required
- An XRite Color Checker Chart. In
some instances, different chart sizes are needed depending on the setup.
- A light meter, a chroma meter (or
both) for monitoring and recording lighting conditions.
- Tripods or mounts as needed to
hold the camera securely at a desired position. Figure 3-1 shows an example of such setup.