SPRAD86A March 2023 – May 2024 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1 , AM67A , AM68A , AM69A
Refer to the AM62A Academy for instructions on adding a sensor driver to the SDK. From the Academy main page, go to Develop Linux on TI EVM → Use Device Drivers → Use Camera → Enable a New CSI-2 Sensor.
In addition to adding the sensor driver to the SDK, the GStreamer plug-ins for the ISP need to be updated to support the sensor. This involves modifying and rebuilding two components in the target file system on the EVM, which is described in the following sections.