This application note presents a series of benchmarks measuring performance of various components of AM62Ax family of devices. Some of the standard benchmarks are included in the Linux SDK while the others can be downloaded from their respective hosting websites. Instructions on how to execute the tests and analysis of the results are also included.
Arm® and Cortex® are registered trademarks of Arm Limited (or its subsidiaries) in the US and/or elsewhere.
CoreMark® is a registered trademark of Embedded Microprocessor Benchmark Consortium.
All trademarks are the property of their respective owners.
AM62Ax contains up to four Arm®-Cortex®-A53 cores with 64-bit architecture, a Cortex-R5F MCU core, a Cortex-R5F Device Management core, a single core C7x256v DSP with MMA, and various other accelerators such as Video and Vision processing, display interface with extensive peripheral and networking options. It supports LPDDR4 32-bit width with speed of 3200 MT/s. #FIG_YMH_MB4_QWB is a functional block diagram for AM62Ax. For details, see AM62Ax Sitara Processors Data Sheet.
This document presents a number of industry standard and application specific benchmarks measured on the AM62Ax processor. The tests focus on the performance of the Arm-Cortex-A53 cors and the LPDDR4 memory with some application specific benchmarks for the Arm-Cortex-R5F MCU, C7x DSP core, and other memory components. The key parameters of the evaluation board are 1.25 GHz and 1.4 GHz clock speed for the Arm-Cortex-A53 cores, 1.0 GHz clock speed for the C7x DSP, and a 32-bit wide LPDDR4 at a speed of 3200MT/s. Most of the standard benchmarks are already included in the SDK and can be directly executed while the other benchmarks can be downloaded from their respective official host websites. All of the benchmarks are implemented using Linux SDK 8.06.
Maximum frequency of A53 cores on AM62Ax varies based on speed grade of the device and the VDD_CORE voltage applied. AM62A SK-LP EVM Rev E2 supports 0.75 V VDD_CORE mode operation which supports operation of maximum core frequency of 1.25 GHz. To obtain peak performance of the device, the setup was modified to run the A53 cores on AM62Ax at 1.4 GHz.