There are a few things to consider when choosing a flash part for application purposes. This document covers some of the basic requirements that a specific flash memory must support to be compatible with the AM273x device during both boot operation and application execution.
The QSPI flash memory can be utilized two different ways in the user system:
When picking a flash memory IC, the device must comply with all boot requirements of the SoC. If the memory is used as boot media, some guidelines must be followed to work efficiently as a storage device during application.
Figure 1 depicts the flash memory organization once the secondary bootloader (SBL) image and valid application image are present.
Figure 2 shows the Boot Flow process where the flash usage is put into perspective, assuming a valid image is already present in flash.
As Figure 2 illustrates, the boot flow process is a sequence adopted by AM273x that starts upon power-on. ROM code is already set to work in a certain way and expects specific instructions from the flash and also expects specific timing and framing configurations for establishing communication. For the AM273x device, ROM code expects the following support:
All of this information is available in the data sheet of the flash device being evaluated. A flash device must support all of the points mentioned above to meet AM273x compatibility requirements.
Application-specific requirements tend to be more lenient then the ROM code execution requirements because improper configuration and lack of support do not result in system boot failure. The following requirements must be met for general flash applications:
The following list includes a few things to consider when deciding on what flash part to use for the application:
The MCU PLUS SDK comes with default flash software support for specific flash memories in the library. If the evaluated flash meets requirements but does not have compatible software drivers in the SDK, use the following link for instructions on how to add support for the flash memory.
The following list shows devices that meet the requirements for correct operation with the Sitara MCU AM273x devices as per the information contained in the data sheets. This list is be used for reference only:
MCU – Microcontroller Unit
QSPI – Quad Serial Peripheral Interface
SoC – System on a Chip
UART – Universal Asynchronous Receiver-Transmitter
SBL - Secondary Boot loader
ROM – Read-only memory
SFI – Serial Flash Interface
SDK – Software Development Package
TI PROVIDES TECHNICAL AND RELIABILITY DATA (INCLUDING DATASHEETS), DESIGN RESOURCES (INCLUDING REFERENCE DESIGNS), APPLICATION OR OTHER DESIGN ADVICE, WEB TOOLS, SAFETY INFORMATION, AND OTHER RESOURCES “AS IS” AND WITH ALL FAULTS, AND DISCLAIMS ALL WARRANTIES, EXPRESS AND IMPLIED, INCLUDING WITHOUT LIMITATION ANY IMPLIED WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR PURPOSE OR NON-INFRINGEMENT OF THIRD PARTY INTELLECTUAL PROPERTY RIGHTS.
These resources are intended for skilled developers designing with TI products. You are solely responsible for (1) selecting the appropriate TI products for your application, (2) designing, validating and testing your application, and (3) ensuring your application meets applicable standards, and any other safety, security, or other requirements. These resources are subject to change without notice. TI grants you permission to use these resources only for development of an application that uses the TI products described in the resource. Other reproduction and display of these resources is prohibited. No license is granted to any other TI intellectual property right or to any third party intellectual property right. TI disclaims responsibility for, and you will fully indemnify TI and its representatives against, any claims, damages, costs, losses, and liabilities arising out of your use of these resources.
TI’s products are provided subject to TI’s Terms of Sale (www.ti.com/legal/termsofsale.html) or other applicable terms available either on ti.com or provided in conjunction with such TI products. TI’s provision of these resources does not expand or otherwise alter TI’s applicable warranties or warranty disclaimers for TI products.
Mailing Address: Texas Instruments, Post Office Box 655303, Dallas, Texas 75265
Copyright © 2024, Texas Instruments Incorporated