This white paper uses the example of a driver monitoring system (DMS) to explain the fundamental elements required to build a safety certifiable system based on Texas Instruments AM62A device and Green Hills® Software’s INTEGRITY® real-time operating system (RTOS).
Sitara™ is a trademark of Texas Instruments.
Green Hills® and INTEGRITY® are registered trademarks of Green Hills Software.
Arm® and Cortex® are registered trademarks of Arm Limited.
All trademarks are the property of their respective owners.
Driver Monitoring Systems (DMS) are subset of so-called interior sensing systems which can use one of several sensor types to gather information about what is going on inside a vehicle. While in most cases infrared cameras are used, there are companies using other methods, for example, radar sensors or even simpler technologies like resistor-mats (to detect whether the passenger seat is occupied by a person or a bag). DMS were first introduced around 2006 and are defined by the European Union (regulation 2019/2144) which states: Driver drowsiness and attention warning means a system that assesses the driver’s alertness through vehicle systems analysis and warns the driver if needed.
Since then, predominantly driven by the industry trend of driver assisted and autonomous driving, a lot of effort has been put into DMS to not only detect and monitor driver distraction (and or drowsiness), but also cover aspects like eye-gaze and even driver emotions to make sure the driver is ready to take over vehicle controls when necessary. Therefore, specifically for higher levels of automated driving – referring to SAE Level 3 and higher – knowing the state the driver is in, is vital for the safety of the vehicle.
Suppliers of DMS have to tackle various problems to make sure the product meets both regulations and market expectations:
With the obvious interdependencies between these areas choosing the correct hardware and software platform can be a challenging task.