SPRADG8 March   2024 AM68 , AM69

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2AM68 Processor
  6. 3AM69 Processor
  7. 4Use Cases on AM68 and AM69
    1. 4.1 HMI
    2. 4.2 Controllers and PLC – Programmable Logic Controller
    3. 4.3 Industrial PC (IPC), Single Board Computers (SBC), and Modules
  8. 5Software Tools and Support
    1. 5.1 Linux Software Development Kit (SDK)
    2. 5.2 SDK Demonstrations and Benchmarks
      1. 5.2.1 TI Apps Launcher
      2. 5.2.2 Seva Store
      3. 5.2.3 Wi-Fi Demo
    3. 5.3 Training Academy
  9. 6Conclusion
  10. 7Relevant Links
  11. 8References

Wi-Fi Demo

The AM68 and AM69 SK board have a PCIe M2E Key interface port which is connected to an Intel-9260 Wi-Fi card. Using this, a Wi-Fi demo can be set up such that the board can act as both a Wi-Fi Access Point (AP) or a Wi-Fi Station that can connect to an external access point like a router or hotspot when powered up. The board also starts iperf3 automatically on the access point interface, and the user can run iperf3 on their devices to test the throughput. Refer to the SDK documentation for AM68 and AM69 for details on this.