The total supported data throughput of
all connected cameras depends on the CSI-2 bandwidth and the ISP bandwidth.
- For the AM6x devices that do not
have an ISP such as AM62P, the CSI-2 bandwidth, 1.5Gbps per lane or 6Gbps for 4
lanes, is the limiting factor. As long as the total data bandwidth of all
cameras is below 6Gbps, this can be supported.
- For the AM6x devices with an ISP
such as AM62A, the ISP bandwidth is the limiting factor. The ISP bandwidth of
the AM62A is 315MPixel/s. As long as the total data rate of all cameras is below
315MPixel/s (regardless of the raw data bit-depth), this can be supported. The
total supported camera data throughput also depends on system load such as DDR
bandwidth. The Performance Analysis section presents the DDR usage for a
specific example as a reference.