- You can refer MCUSDK documentation to flash generated binary into OSPI
using section
- If the pcie_enumerate_ep example
is started on an AM24x EVM that is NOT connected to an x86 RC, or if the x86 is
not powered, the only output is going to be:
- Power off AM64x and
Linux-PC
- Power on AM64x having
pcie_enumerate_ep flashed
Afterward, the sample application is waiting for a
PCIe link to be established, which requires the RC. Once the cable is connected and
the RC is powered, the application outputs the state changes: