SPRADJ1A June 2024 – August 2024 TMS320F280021 , TMS320F280023 , TMS320F280023C , TMS320F280025 , TMS320F280025C , TMS320F280033 , TMS320F280034 , TMS320F280037 , TMS320F280037C , TMS320F280039 , TMS320F280039C , TMS320F280041 , TMS320F280041C , TMS320F280045 , TMS320F280049 , TMS320F280049C , TMS320F28075 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377S , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379S , TMS320F28P550SJ , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK
Figure 2-1 is a simplified schematic diagram of an LLC converter with HHC scheme. Compared to the voltage mode control, it is required to sense the voltage of resonant capacitor (VCR) and control the swing amplitude for HHC, which works as an inner loop in addition to the voltage control loop. Similar to the peak current control, the VCR control is used to controlling the energy transferred from resonant tank to the output for LLC. For the VCR sensing circuits, it can also leverage the existed current sense transformer, which is explained in the later section.
Figure 2-2 shows the HHC control architecture within the C2000 MCU, which includes the outer voltage loop and hardware-based VCR loop. The voltage loop compensator generates the control value to the ramp generator of comparator subsystem module (CMPSS), based on the error from sensed voltage and reference voltage. The CMPSS compares the sensed VCR voltage with the ramp generator value, and generates events to control the PWM signal for the high side FET. CLB is used to create the PWM signal for the low side FET with a specific logic from the high side PWM.
Different from the traditional peak current mode control on buck, boost or phase shift full bridge topologies, which run with fixed switching frequency, while HHC LLC implements the peak current mode control for variable switching condition. Figure 2-2 shows the HHC switching waveform. When the VCR voltage swings up and comparator event is triggered, the high side FET can be turned off, and the low side FET can be turned on. In the later half cycle, the low side FET’s on-time is kept as the same as the high side FET’s. Similar with peak current mode control, a compensating slope is added to keep the control loop stable during the light load, when the VCR swing amplitude is very small.
Figure 2-3 shows the block diagram of the HHC control logic, which mainly includes three peripherals of C2000.