SPRADN4 December 2024 AM62P , AM62P-Q1
WKUP_LFOSC0 has limited use cases and is optional. Based on the use case, select a 32.768kHz crystal as the clock source or a 1.8V LVCMOS square-wave digital clock source.
For more information, see the [FAQ] AM625: LFOSC usage in the device. The FAQ is generic and can also be used for AM62P / AM62P-Q1 processor family.
Place all discrete components used to implement the oscillator circuit as close as possible to the WKUP_LFOSC0_XI and WKUP_LFOSC0_XO pins. For the crystal, the load capacitance selected is required to be in the range recommended in the WKUP_LFOSC0 Crystal Electrical Characteristics table of the processor-specific data sheet.
If WKUP_LFOSC0_XI / WKUP_LFOSC0_XO is not used, recommended is to connect the XI directly to the VSS and to leave the XO unconnected.
For more information on connecting the unused WKUP_LFOSC0, see the WKUP_LFOSC0 Not Used section of the processor-specific data sheet.