SPRADN4 December 2024 AM62P , AM62P-Q1
Peripherals that have a dedicated function have connectivity requirements when not in use. Refer to the Pin Connectivity Requirements section of processor-specific data sheet for connecting unused peripherals. The connectivity requirements include recommendations to connect the power supply and the interface signals.
Peripherals that have alternate functions that are not used can be left unconnected when there are no connectivity requirements specified. The pad configurations can be the reset configuration.