SPRADN4 December 2024 AM62P , AM62P-Q1
The VBUS power is sourced by an external host. USB standard for device operation recommends connecting < 10μF capacitor to the VBUS close to the USB Type-B connector.
Follow the USB VBUS Design Guidelines section of the processor-specific data sheet to scale the USB VBUS voltage (supply near the USB interface connector) before connecting to USBn_VBUS pins.
Based on the use case, the zener diode can be deleted if the user is absolutely sure that the board never experiences a VBUS signal potential greater than 5.5V (sourced on-board).