SPRADO2 November 2024 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1
Recommend adding required design notes for the processor peripherals (Example: USB2.0 interface, Ethernet interface, Camera interface, eMMC, OSPI, SD, and other available processor peripherals). Notes added can include Board Boot mode configurations, placement of series and parallel resistors, placement of decoupling and bulk capacitors.
Consider adding the required or applicable design notes to the processor attached devices and on-board devices. Adding notes helps understand the implementation rationale.
Mark all differential signals, critical signals and specify the target impedance (as required). See the following examples:
See the following FAQs:
[FAQ] AM625: PCB Pattern Recommendations for Specific Peripherals
[FAQ] AM625: MMC0 PCB Connectivity Requirements
AM6442: PCB layout guidelines for MMCSD0(eMMC) and MMCSD1(SD card)