SPRADO2 November 2024 AM62A3 , AM62A3-Q1 , AM62A7 , AM62A7-Q1
For the operation of the processor, select a crystal as the clock source or a 1.8V LVCMOS square-wave digital clock source.
A 25MHz external crystal connected to the internal high frequency oscillator (MCU_HFOSC0) is the clock source for the internal reference clock HFOSC0_CLKOUT.
Placed the discrete components used to implement the crystal oscillator circuit as close as possible to the MCU_OSC0_XI and MCU_OSC0_XO pins. For the crystal, follow the MCU_OSC0 Crystal Circuit Requirements table of the processor-specific data sheet when choosing the load capacitors.
When a 1.8V LVCMOS square-wave digital clock source is used, connect the processor XO pin according to the processor-specific data sheet recommendation.
For information on clock selection, refer to [FAQ] AM625, AM623 / AM625SIP, AM625-Q1, AM620-Q1 Custom board hardware design – Queries regarding Crystal selection. The FAQ is generic and can also be used for AM62A7 / AM62A3 / AM62A7-Q1 / AM62A3-Q1 processor family.
Refer to [FAQ] AM625 / AM623 / AM625SIP / AM625-Q1 / AM620-Q1 Custom board hardware design – Queries regarding MCU_OSC0 Start-up Time. The FAQ is generic and can also be used for AM62A7 / AM62A3 / AM62A7-Q1 / AM62A3-Q1 processor family.
25MHz is the only crystal frequency that is currently supported. See the processor-specific data sheet for more details on the crystal parameters.
The next revision of the data sheet includes LVCMOS clock requirements as part of the MCU_OSC0 LVCMOS Digital Clock Source section. Refer section 3.1 Data Sheet Use Case and Version References in the Application Note of the application note.