SPRSP63B October 2022 – November 2023 TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137
PRODUCTION DATA
This section explains the default boot modes, as well as all the available boot modes supported on this device. The boot ROM uses the boot mode select, general-purpose input/output (GPIO) pins to determine the boot mode configuration.
Table 7-6 shows the boot mode options available for selection by the default boot mode select pins. Users have the option to program the device to customize the boot modes selectable in the boot-up table as well as the boot mode select pin GPIOs used.
All the peripheral boot modes that are supported use the first instance of the peripheral module (SCIA, SPIA, I2CA, CANA, and so forth). Whenever these boot modes are referred to in this chapter, such as SCI boot, it is actually referring to the first module instance, which means the SCI boot on the SCIA port. The same applies to the other peripheral boots.
See the Reset (XRSn) Switching Characteristics table and the Reset Timing Diagrams for tboot-flash, the boot ROM execution time to first instruction fetch in flash.
BOOT MODE | GPIO24 (DEFAULT BOOT MODE SELECT PIN 1) |
GPIO32 (DEFAULT BOOT MODE SELECT PIN 0) |
---|---|---|
Parallel IO | 0 | 0 |
SCI / Wait Boot(1) | 0 | 1 |
CAN | 1 | 0 |
Flash | 1 | 1 |
BOOT MODE NUMBER | BOOT MODE |
---|---|
0 | Parallel |
1 | SCI / Wait |
2 | CAN |
3 | Flash |
4 | Wait |
5 | RAM |
6 | SPI |
7 | I2C |
10 | Secure Flash |