SPRU513Z August 2001 – October 2023 SM320F28335-EP
The copy table format is the same irrespective of the compression_kind. The size field of the copy record is overloaded to support compression. Figure 8-7 illustrates the compressed copy table layout.
In Figure 8-7, if the size in the copy record is non-zero it represents the size of the data to be copied, and also means that the size of the load data is the same as the run data. When the size is 0, it means that the load data is compressed.