SPRU514Z July 2001 – October 2023 SM320F28335-EP
Any vendor who wishes to distribute a library that can be rebuilt automatically by the linker must provide:
These things must be placed together in one directory that is part of the linker's library search path (specified either in C2000_C_DIR or with the linker --search_path option).
If mklib needs extra information that is not possible to pass as command-line options to the compiler, the vendor will need to provide some other means of discovering the information (such as a configuration file written by a wizard run from inside CCS).
The vendor-supplied mklib must at least accept all of the options listed in Table 8-2 without error, even if they do not do anything.