SPRUHM8K December 2013 – May 2024 TMS320F28374D , TMS320F28375D , TMS320F28376D , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28378D , TMS320F28379D , TMS320F28379D-Q1
During boot ROM execution, there are situations where the CPU can enter a wait loop in the code. This state can occur for a variety of reasons.
Table 4-14 gives the address ranges that the CPU1 PC register value falls between, if the boot code has entered one of these instances. Table 4-15 gives the addresses for CPU2.
Address Range | Description |
---|---|
0x003F E2D4 – 0x003F E2EF | In Wait Boot |
0x003F E73E – 0x003F E824 | In NMI Handler (startup) |
0x003F E35A – 0x003F E468 | In NMI Handler (PIE) |
0x003F E468 – 0x003F E495 | In ITRAP ISR |
Address Range | Description |
---|---|
0x003F E44C – 0x003F E451 | In Idle Mode |
0x003F DEAA – 0x003F DFC2 | In NMI Handler |
0x003F DE61 – 0x003F DEAA | In PIE Vector Mismatch Handler |
0x003F DFC2 – 0x003F E00B | In ITRAP ISR |