SPRUI03E June 2015 – January 2023
Initialize Bits
.bitsvalue[, size in bits]
The .bits directive places a value into consecutive bits of the current section.
The .bits directive is similar to the .field directive (see .field topic ). However, the .bits directive does not force the value to be aligned to a field boundary. If the .bits directive is followed by a different space-creating directive, the SPC is aligned to an appropriate value for the directive that follows.
This directive has two operands:
"t.asm", WARNING! at line 1: [W0001] Value truncated to 1
.bits 3, 1