SPRUI25D June 2015 – March 2019 TMS320F28374S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379S
Including the LaunchPad demo example described above, controlSUITE provides many examples demonstrating a majority of the features of the F2837x MCU. Most examples are configured by default to use the other hardware which has a different on-board clocking circuit. As such, some examples may not work as intended without minor modification. To make this easier on the designer, compiler switch has been added to automatically pick the proper clock configuration based on adding "_LAUNCHXL_F28377S" as a predefined symbol in the project properties. Refer to for more information on how and where to define this symbol.