SPRUI30H November 2015 – May 2024 DRA744 , DRA745 , DRA746 , DRA750 , DRA756
NMI is the second-highest priority interrupt and is generally used to alert the CPU of a serious hardware problem. For an NMI to be detected (and processed) by the ARP32 CPU, the non-maskable interrupt enable (NMIE) bit in the interrupt enable register (IER) must be set to 1. The NMIE bit is cleared to 0 at reset to prevent an NMI being taken prematurely (before system initialization). The NMI bit is set (to enable NMI) by software only after the system has been properly initialized and is ready to accept NMIs. The NMIE bit is also cleared at the occurrence of an NMI to prevent another NMI from being processed; it may be set again in the interrupt set register (ISR), to allow nested NMIs, by software after the CPU state has been saved properly in the previous NMI ISR. While the NMIE bit is cleared, all maskable interrupts (INT15–INT4) are also disabled.
When the NMIF bit is set, (as a result of an NMI assertion via cpu_nmi_i input pin), assuming the previous conditions are met, the ARP32 CPU is said to accept the interrupt and performs the following actions to process the NMI:
To exit an NMI service routine, the BNRP instruction must be used. Execution of the BNRP instruction causes: