SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
The YC 4:4:4 data type is used for interleaved 4:4:4 data. It is expected to be packed with Y0 in the lowest byte followed by Cb followed by Cr. The transfer counts each YCbCr triplet in a 24 bit word as a pixel. A 2D transfer of the data is NOT supported in the VPDMA. The data block width and height should be set to the number of pixels and lines that are expected by the client.