SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
Bits 15:0 are the stride between lines in bytes at the external address. This value is added or subtracted based upon an adjustment using the current skip value. Operation of the external address pointer shall load the Source Address upon start of the transfer, then at the end of each line increment or decrement by the value computed using the Line Stride and Skip value for the line. The line stride must be aligned to an L3 data bus width. The lower bits of the stride will always be treated as zero to force the alignment.