This event is registered on the following error conditions:
- One or more of the following errors are registered during a non-data FIS transfer:
- Protocol (SATA_PSERR[10] ERR_P)
- CRC (SATA_PSERR[21] DIAG_C)
- Handshake (SATA_PSERR[22] DIAG_H)
- SATA_PHY not ready (SATA_PSERR[9] ERR_C)
- Command list underflow during a read operation when software builds a command table that has more total bytes than the transaction given to the device
Note: The conditions previously described are non-fatal and the SATA host controller continues to operate normally.