Errors are generated if enabled under three conditions:
- EDMA_TPTC detection of an error signaled by the source or destination address.
- Attempt to read or write to an invalid address in the configuration memory map.
- Detection of a constant addressing mode TR violating the constant addressing mode transfer rules (the source/destination addresses and source/destination indexes must be aligned to 32 bytes).
Either or all error types may be disabled. If an error bit is set and enabled, the error interrupt for the concerned transfer controller is generated.