SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
EDMA_TPCC_CIDX_n[31:16] DCIDX is a 16-bit signed value (2s complement) used for destination address modification in the 3rd dimension. Valid values are between –32 768 and 32 767. It provides a byte address offset from the beginning of the current array (pointed to by DST address) to the beginning of the first destination array TR in the next frame. It applies to both A-synchronized and AB-synchronized transfers.
When DCIDX is applied, the current array in an A-synchronized transfer is the last array in the frame (Figure 16-19), while the current array in a AB-synchronized transfer is the first array in the frame (Figure 16-20).