The DSP_SYSTEM module controls the following functions:
- Generation of the divided clocks (DSP_CLK2 or DSP_CLK3) to all components of the DSP subsystem
- Synchronization of the DSP divided clocks
- PRCM module power handshaking
- Reset input resynchronization of the active-to-inactive transition to the CD1_CLK clock
- DSP subsystem top level configuraiton registers and its access from the DSP core.
Figure 5-3 highlights the DSP_SYSTEM and its connectivities to the surrounding blocks within the subsystem and in the device.