SPRUI30H November 2015 – May 2024 DRA745 , DRA746 , DRA750 , DRA756
The device can boot to invoke WIR mode. If the device is booted in this mode, all processors within the device that support a TAP through ICEPick are held in reset until released. Individual processors can be released from reset (local), or all processors held in the reset state can be released at the same time (global).